Dear Sir/Ms.
How to calculate the Min on time of TPS562201? I only found the Min. off time in the data manual about 220ns.
My colleague's client specs are as follows
Fsw Switching frequency VIN = 12 V, VO = 1.05 V, FCCM mode 580 kHz
I am afraid that the IC will trigger the Min on time and cause the output voltage to be unstable.
I need the Min. on time of TPS562201.
Best Regards,
Kami Huang