Dear Team,
I am looking for a competing product of MP3363.
The required specifications are as follows.
Vin=6V~9V
Vout=18V
Iout=20mA
External Synchronization or adjustable Switching Frequency
Best regards,
Luna
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI Luna,
How about TPS61500? Could you help introduce the application where MP3363 is used? Thanks.
Robin
Dear Frank Qiu and Robin,
Thank you for the information.
The functionality of the TPS61500 meets the requirements. However, the application is a camera, so a small package is ideal.
Best regards,
Luna
Hi Luna,
There is no smaller device with adjustable switching frequency. Why customer need configurable switching frequency?
Robin
Hi Robin,
Thank you for your reply.
This application uses multiple switching regulators.
I would like to make adjustments to avoid interference at their respective switching frequencies.
Best regards,
Luna