Other Parts Discussed in Thread: LP8764-Q1, TPS6593-Q1,
This is relevant to TPS6593-Q1, TPS6594-Q1, LP8764-Q1, TPS6594x devices, and LP876x devices.
I2C addresses for your first device can be any valid value defined by the 7-Bit address ID. However, because of the device’s 4 pages of I2C registers, the next three addresses should be unoccupied. For instance, if the device address is 0x48, the next highest device address on the bus should be 0x4C. This includes other PMICs. Common default I2C addresses for PMICs are 0x48, 0x4C, 0x50, and 0x58.
----------------------------------------------------------------------------------------------------------------------
Looking for more help? [FAQ] List of FAQs for TPS6594-Q1, TPS6593-Q1, LP8764-Q1 PMICs