Other Parts Discussed in Thread: LP8764-Q1, TPS6593-Q1,
This is relevant to TPS6593-Q1, TPS6594-Q1, LP8764-Q1, TPS6594x devices, and LP876x devices:
The Real Time Clock function (RTC) provides a method by which the PMIC’s enabling and sleep can be configured to be based on alarms and timers. These could be used to submit on and off requests which may be useful to an application. Though useful, this function is not required to utilize the rest of the PMIC.
----------------------------------------------------------------------------------------------------------------------
Looking for more help? [FAQ] List of FAQs for TPS6594-Q1, TPS6593-Q1, LP8764-Q1 PMICs