Hi
I'm not going to use a VDDM pin.
So I just need to connect the cap to VDDH and VSSS?
Can I open VDDM?

Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I'm not going to use a VDDM pin.
So I just need to connect the cap to VDDH and VSSS?
Can I open VDDM?

Thanks
Hi David Kim2,
Thank you very much for reaching out.
CDIV1 and CDIV2 act as bootstrap capacitors where CDIV2 charges to 5V (VDDM) and CDIV1 charges 5V above VDDM producing a 10V rail (VDDH) with reference to VSSS. These two capacitors are required for the device to function properly. In addition, VDDH has a UVLO that will assert VDRV low if triggered.
Let us know if this answered your question.
Sincerely,
Francisco Lauzurique