Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1H100-Q1: TPS1H100-Q1

Part Number: TPS1H100-Q1

Hi,

Please provide us the complete electrical parameter details such as -  IOH,IOL,VIH,VIL,VOH,VOL,IIH,IIL for the PART TPS1H100-Q1.

Regards

Kaushik 

  • Kaushik,

    For this device (since it is built as a switch with the express purpose of providing DC power from source to load), the parameters of concern are the V_ih and V_il. 

    You can find these on the datasheet here:

    If the part is powered, any voltage over 2V on the IN pin will result in the part turning ON, any voltage lower than 0.8V will result in the part turning off.

    DC operating between 2V and 0.8V on the IN pin is NOT recommended.

    Thanks,

    Shreyas