This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV700: EN pin connection

Part Number: TLV700

Hello,
Those written in the datasheet for the EN pin;
"Enable pin. Driving EN over 0.9 V turns on the regulator. Driving EN below 0.4 V puts the regulator into shutdown mode and reduces operating current to 1 μA, nominal.

The enable pin (EN) is active high. The device is enabled when voltage at EN pin goes above 0.9 V. The device is turned off when the EN pin is held at less than 0.4 V. When shutdown capability is not required, EN can be connected to the IN pin."
According to this, should I make a connection like in the picture?
Vcc from the battery connector should be connected as Vin here, right?
Thanks in advance.