Other Parts Discussed in Thread: BQ25180, PTH04T241W
Hello,
We are using the TPS54910 to drive a heating element requiring a supply voltage of 2.4V and consumes up to 8A.
The TPS54910 is supplied directly from a a high discharge Li-ion Battery 3.7V /1000mAh, this battery is charged using a BQ25180 through USB.
Knowing that the system output of the BQ25180 can only supply maximum of 2.5 A, we connected the buck converter to the Battery directly.
TPS54910 will be disabled in from the main controller in case the battery voltage is low.
Can you please advice if such setup is adequate or do you recommend other options.
We tried to simulate the configuration of the TPS54910 using the WEBENCH, it turned out that it is not supported, are their any other method to simulate the configuration?
Best Regards