Hello,
I am now trying to use a LP87524 q1 DC DC converter to convert a voltage from 5V into 3.3V, 2.7V, 1.8V and 1.2V. And because 4 different output voltages are needed, I will choose the configuration of four 1-phase outputs.
But now I have a problem, the current of the load that I intend to connect after the 1.2V output is pretty big, about 3A. I want to ask if this output can bear a current of 3A, what is the maximum current output of one single phase in the four 1-phase configuration?
In the datasheet it's actually written that when input voltage is bigger than 3V, then the maximum output current of a single phase in 1-phase configuration is 4A, but the output voltage is not really specified in this term. I actually want know, when the output voltage is fixed as 1.2V, what is the maximum current output then?
thanks a lot in advance!
Best regards
Max