Part Number: BQ24166
Hello,
I use the BQ24166 in my Design.

Charging with a USB-Source works fine. Even if current is taken from the system at the same time. The USB-Current is always this what is configured with IUSB1-3 (1500mA).
This is not the case for the "In" Input:
- I Limited I_Lim to max 1,76A (150 Ohm resistor)
- The Charge-Current is limited to max 1,63A (330 Ohm resistor)
=> I expect that my power supply will now not be loaded with more than 1.76A. But it will be 2,25A. The BQ24166 will get extremly hot.

what is still noticeable:
If it is charging via "In" and there is no system-load connected, it seems all good.
But if i connect the system, the "In"-Current is raising slowly, into the finite. The BQ24166 gets very hot. The faster it gets hot, the more the current rises.
If I cool the Chip down, the "In" current decreases to the start value.
As long as the chip is "cold" it looks like the I_lim is working good.
Here a Video:
(You can see me using cooler-spray)
Do anyone have an idea why?