I already asked what is the maximum output power possible.
I understand your answer that it depends on external power components and magnetics.
I am copying the below statement from data sheet (page 21):
The output of the voltage-error amplifier (VVAO) is clamped at 5 V, which represents the maximum PFC output
power. This value is used to calculate the maximum reference current at the IMO pin, and sets a limit for the
maximum input power allowed (and, as a consequence, limits maximum output power).
It looks like maximum voltage of VAO limit the output power.
I asked what is the maximum output power possible with respect to above statement.
Kindly clarify.