This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3409: Capacitive load

Part Number: LM3409


Hello everybody,

does the LM3409 will function properly if there is a capacitive load (1000µF) on the output, so in parallel with led.

Thanks a lot in advance.

  • Hello,

    You can consider the LM3409 as a current source, so this would be like feeding a constant current into a parallel combination of capacitor and LED. The capacitor will reduce the current ripple flowing into the LED. Normally the large capacitor is fine, unless you are doing specific things. For example if you plan to use bypass/shunt dimming the large capacitor is not recommended. 

    -Sumeet