Hi,
In my board I use 3 devices from TPS62913 types.
How should I connect them to prevent as much as I can EMI issues?
First DCDC:
VIN = 9V; VOUT = 1V @ 1.5A
Second DCDC:
VIN = 9V; VOUT = 3.6V @1.3A
Third DCDC:
VIN = 9V; VOUT =5V@ 1A.
The first and second DCDC always on and the third selected with EN.
Can I sync them without external clock?
Thanks