Other Parts Discussed in Thread: BQSTUDIO, GPCCHEM
I'm attempting to complete a learning cycle on a BQ40z80 battery gauge as detailed on SLUA848 application report.
No problems completing successfully the sequences detailed in par. 4.2.1 (discharge to empty), 4.2.2 (Relax for at least 5h),
4.2.3 (Charge battery to full).
But when doing what is detailed on 4.2.4 paragraph (Relax for at least 2h) what I'm observing is that the BQ40z80
sets correctly the REST flag indicator, but it doesn't advance its LStatus() from 0x4 to 0x5 as pointed out in the application report.
What to do now?
I've to restart the whole procedure one more time? And why, i.e. which is the missing step that doesn't permit the LStatus() increment to 0x5 value?
Thanks in advance to all,
Simone.