Hello Team,
The TPS25947 is UL2367/IEC62368-1 compliant, but I'd like to confirm for my understand the current limit setting for the standard.
The ITIMER can be set to allow transient peak currents on the TPS25947, but the standard seems to require that the current be kept within 15VA. (IEC62368-1)
If standard based design is required, should the current limit be set to take into account the transient peak current?
Best regards,
Sato