From the SLUSE81C document, does UT_THR = b111 mean 66% TSREF?
If OT_THR= b00000, is this 39% TSREF?
Based on this assumption, an OT threshold of 16% TSREF and UT threshold of 80% TSREF will be 0x17. Please confirm.
If OTCB_THR = b1111 is this 24% TSREF
If COOL_OFF = b000, is this 14% TSREF?
Based on this understanding, OTCB_THR = b1101 is 20% TSREF
if COOL_OFF = b101, this is 4% TSREF. Please confirm.
Thanks