This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100: Cycle count issue

Part Number: BQ34Z100
Other Parts Discussed in Thread: BQ40Z50

Hi team,

The customer would like to know what's the difference between Configuration-Date-Cycle Count and Gas Gauging-State-Cycle count. Could you help resolve this case? Thanks.

Best Regards,

Cherry

  • Hello Cherry,

    The configuration-data cycle count is the actual cycle count reported by the SBS command and represents the actual number of cycles.

    The Gas Gauging-state cycle count represents the cycle count at the last Qmax update. The two values are used to calculate the MaxError() reported by the gauge from the last successful learning.

    Sincerely,

    Wyatt Keller

  • Hello Wyatt,

    Thanks for your help.

    Can the soc be configured to 100%? And can it be configured to keep the SOC at 99% if the full charge condition is not met?

    Thanks and regards,

    Cherry

  • Hello Cherry,

    The SOC can't be manually adjusted, the gauge is constantly updating the SOC value according to the Impedance Track algorithm.

    You can't force the SOC to stay at 99% like some of the other gauges (BQ40Z50) until valid charge termination. The feature is not supported.

    Sincerely,

    Wyatt Keller