Part Number: BQ25790EVM
Following along with the User Guide I have made my way to Section 2.4.3.3 and note that I am not measuring " IBAT_SENSE (voltage across 0.01 ohm resistor between TP17 and TP18) = 240 mA ±60 mA"
Furthermore it looks like I'm seeing flickering faults on VBAT_OVP_STATUS and VSYS_OVP_STATUS. From playing around with the order of operations, it seems I need to have my battery simulator enabled prior to turning on PS #1, else I enter this fault state. The guide, in Section 2.4.3.1 simply says they both should be on from Section 2.4.1, which says to turn them both on in 2.4.4 but in no particular order.
The guide Section 2.4.3.2 states that I should have both PS #1 and Load # 1 ON, then reinstall the J19 jumper (Section 2.4.3.2) to enable charge. This order of operations causes the faults mentioned above.
What seems to work is to have only Load # 1 ON (a battery simulator) with jumper J19 installed, then turning on PS #1. Any other order seems to result in some faults and no charge occurring.
Any hints as to why this is the case?