This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Fast Charging solution for Li-Ion Battery Using USB-C

Other Parts Discussed in Thread: TPS25750

Dear Sirs

We need to design a fast charging solution for a  1000mAH Li-ion battery (attached datasheet)

Appreciate if you can propose best charging chip enabling Fast charging  via USB-C

Best Regards

Elias


LPHD7425048 1000mAh.pdf

  • Hi Elias,

    What is the total system load and charging current you would like to support?

    If you would like to use the USB-PD protocol, we recommend the TPS25750 and...

    • If you are designing a battery powered system for 45 W and below please consider BQ25792 or BQ25790
    • If you are designing a battery powered system for 45 W and above please consider BQ25731

    Do you need the OTG feature? What type of supply do you intend on using for this battery? Can you give me more information about your system setup?

    Regards,

    Mike Emanuel

    Please click "Resolved" if this answered your question.