Other Parts Discussed in Thread: CSD18540Q5B, LM3478, LM5155
Hi, I am looking to design a 240W non-isolated boost converter using LM5156 and do not intend to use the current sense feature of the ASIC. Would it be okay for me to short the CS pin to PGND? Also, if shorting CS to PGND is acceptable what compensation components should be chosen? Can the compensation components be also left out? I am intending to drive the boost at ~440kHz with min. and max. input voltages at 7.5V and 12.6V respectively. Also, output voltage of the boost is expected to be 24V.
Thanks
Rishi