Dear team,
My customer wants to know what the maximum reflow soldering temperature we support is. Could you please help answer it?
Thanks & Best Regards,
Sherry
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear team,
My customer wants to know what the maximum reflow soldering temperature we support is. Could you please help answer it?
Thanks & Best Regards,
Sherry
Hi Sherry,
This device is specified as Level 1 MSL rating as per JEDEC industry standard with a maximum peak temperature of 260°C (+0° / -5°C).
The details of the profile are defined in the standard IPC/JEDEC J-STD-020. Refer to section 5.6 “Reflow”, table 5-2 Classification profiles for Pb-Free Assembly of the standard.
Regards,
Febin