This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27510: BQ27510 I2C Not Detected

Part Number: BQ27510

Hi everyone,

I am using the BQ27510 to monitor a Li-Ion Battery, I have it on a PCB, however, when I went to connect the SDA and SCL to the MCU, the MCU does not detect it. I realized I had placed the pull up resistors incorrectly and fixed the design issue (they are now not in series and are connected to 3.3V, I have not updated the schematic) , however, it is still not being detected. I have attached my design below can someone let me know if there is some design issue I am missing?

Some extra information that might help: I am using a Li-Ion 3.7 V, 4500 mAh battery. I am currently powering a Raspberry Pi 4 with the battery at 5 V and 2.5~3A