Part Number: BQ24072T
The charger IC on my board has stopped charging. I have listed my observations and testing performed so far:
ILIM and ISET read 0V and there is no output current at BAT.
I have checked and tested the following
- Resistor on ILIM and ISET are the correct values
- Measured between pads of resistor, and between IC pin and GND pin to confirm good connection
- No shorts between pins, power and GND
- nPGOOD and nCHG are low (LEDs on)
- OUT is correct value when power adapter is plugged in
- OUT is correct value when only the battery is plugged in
Are there any other tests I can run to determine the cause of failure