We're currently experiencing a small level of fallout with devices using TLV62568ADRL as a 3.3V, 1.0A switching regulator.
The device input is 5V, fed from TI LM2678S-5.0.
Our schematic design based on the datasheet and Web Bench:
On failures we observe that the SW output of the device is shorted to ground.
Replacing the device resolves the issue.
We cannot find any issues farther downstream from devices powered by the 3.3V output.

I suspected possibly an overvoltage event at the Vin pin, but might expect that would damage both of the output devices instead of just the low side FET.
To explore this I tried to forward and reverse bias the body diodes in the output stage on 4 samples (2 good, 2 bad):
My measurements seem to suggest that the high side FET body diodes of the bad samples are intact (blocking reverse voltage), but their forward voltages certainly appear different.
Are there any other suggestions of what may be happening to these devices? ESD bogeyman is a possibility, but I'm trying to think of what else is possible to experimentally rule out.