Part Number: LP8550
Other Parts Discussed in Thread: TPS65132,
Hello,
we have the following requirements for a LCD backlight WLED driver:
* 3s4p configuration (3s2p top, 3s2p bottom), each side has shared anode and separate cathodes per string
* 32mA@5.85Vf per LED, recommended 10% duty cycle. Allowable LED current from 100mA @ 10% duty cycle to 30mA @ 100% duty cycle
* Synchronization to VSYNC (90-120Hz) or HSYNC (2448 * VSYNC). DDIC provides the following outputs:
1. "LEDPWM" out which is a VSYNC-synchronized pulse (delayed by n HSYNC clocks and m HSYNC clocks wide, with n, m user configurable)
2. "TE" out which is high during vertical blanking OR high during vertical blanking for a longer period of time and horizontal blanking for a shorter period of time

* Small form factor (BGA) preferred
This could be integrated with a LCD bias, but is not required (+- 5.8V at +-32mA, TPS65132 seems suitable)