Hi,
We have designed a charging module using BQ2057WSN IC to charge a 8.4V, 2400mAH 2S 18650 Li-ion battery. My supply power is 9V 5W SMPS. I have set my charging current to mA. The battery is charging continuosly and does not cutoff charging even if the pack voltage has reahed 8.4V. But in some of the I found that the IC is showing both the staus indicators of full charged and also in charging at the same time. I have measured the input power supply voltage and found it as 9V which is fine. Then I have measure the battery float voltage accross Pin No. 2 & Ground it is 9.35V. I have found that in some of the circuits it is different. So, what could be possible reasons of getting such unexpected state where it is continuosly charging baterry beyond 8.4V. Is there any flaws in my design or the IC is faulty ( But remember IC is not showing any short circuit).
I also found that out of these circuits,idealy 50% of circuits are facing this issue.
I am attaching my schematic and some images related to the circuit. R1 or R8 is 0.47ohm