This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2962: VC1 connects to VSS

Part Number: BQ2962


Hi team,

Customer use BQ296203 for secondary protection on their 3S Notebook project

If they short connect VC1 with VSS to ground does this have potential risk for PF function and REG output?

Thanks.

  • Hi Steven,

    Normally for 3 cells, most users follow Figure 9-2 in the datasheet which shorts V4 and V3. I think it may be okay to short V1 to VSS, but there is one place in the datasheet that seems to show there is some special significance for the V1-VSS voltage. If possible, they should short V4 to V3 to be safe instead of shorting V1 to VSS.

    Best regards,

    Matt

  • Hi Matt,

    Customer want this connection because they don't want RTC output and under this circumstance V1 will be in low voltage status and RTC doesn't have output. They wonder if they can use this implementation method and whether the protection of V2 V3 V4 will be influenced and the consumption will be affected compared with our recommendation. 

    Currently I recommend them to use our design and connect a 0.47uF capacitor on REG pin since they don't use the REG output. But they still want us to clarify the above questions. Thanks for your help.

  • Hi Steven,

    Ok, I understand. I think this is probably not a good idea because if the regulator is turned off, this could possibly affect other internal circuits in the device. It was not designed to operate with the regulator forced off by a low voltage.

    Best regards,

    Matt