This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25173: functional application question

Part Number: BQ25173

hi team:

 there is some questions about the BQ25173 device, would you help to clarify that?  tks for your help.

1.The input voltage is 5V/60mA, and the super capacitor is 2.7V/10F. At this time, if the charging current we design is 80mA, and according to the efficiency of 90%, the remaining input power is 270(5V*60mA *90%)-216(5v*80mA)=54mW, will this remain power loop back to the load?

2.Before the capacitor is fully charged, does the end load of 2.7V comes from the input or the capacitor ?

3.base on the question 2,if  it comes from the input first, when the input power cannot meet the load requirements, will the capacitor be discharge immediately?