This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BMS system solution recommendation

The battery pack is 63V 90AH with '21700' cells. There are 2 types for it, one is 15 cells in series and 18 cells in parallel for one battery pack unit. Another one is a big box and insert 6 battery pack unit in parallel, each battery pack unit consists of 15 cells in series and 3 cells in parallel. Communication via CAN bus protocol.

My questions is

  1. What the different between one unit and 6 unit for balance, charge and discharge?
  2. How to deal with the communication among the 6 6 battery pack unit?
  3. Base on TI the solution and experience, which type is better? Why?
  4. Please base on above to provide the solution? If still need detail information, please let me know.