Has anyone had a problem with excessive input current (>15 ma) at 1 to 1.5 Vin during startup? We have measured a narrow "carrot" region where the TPS 60402 draws nearly 20 mA around 1.28 V during startup. It is unusable in our low power application, which can supply only about 5 to 6 mA. Would like to use this part because of it's 125 C capability, but it does not seem viable unless the power input can supply 20 mA during startup. Tested with Cfly and Cout = 1uF; Cin = 4.7 uF, V in = 5V. Any suggestions? For now, we're using MAX1852, which starts and runs perfectly, drawing < 100uA at all input voltages.