Hello -
We are experimenting with the UCC28712 in a 24V power supply design. We are using a SiC MOSFET as the primary switch in the flyback circuit. During startup, we observed the following waveform where the blue trace is the gate signal, and the yellow trace is the voltage across the primary coil (drain to +DC bus). This shot was taken when input voltage was ~ 100Vdc. As we go up in input voltage, the gate signals eventually all look like the middle one in this screen shot. Any thoughts on what would be causing the gate output to shutoff like this?

Thanks!
Brett