Hi TI experts,
I used the 17Pin of BQ40Z80 as the function button of EMSHUT. For example, when I press the button, the battery turns off the output, and when I press the button again, the battery turns on the output, which is used as the battery on and off key repeatedly. At the same time, the EMSHUT-EXIT-VPACK register is turned on. After pressing the button to turn off the battery output, charging can reactivate the battery and turn on the charge and discharge MOS.


However, in the process of charging and discharging (charging current > discharging current), the customer found that if the button is pressed by mistake, the battery will briefly turn off the output (about 750ms). The electrical appliances are suspended, the experience is not good. So can the button action of the EMSHUT function be shielded during the charging process?It is required that the output of the battery is not turned off during charging.

Looking forward for your reply, thank u.