This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116EVAL: how to modify to change I/P to take upto 95VDC and O/p Current upto 9A?

Part Number: LM5116EVAL
Other Parts Discussed in Thread: LM5116

Dear E2E Forum,

  I need to use LM5116EVAL/NOPB

I need minor modification as per my requirement given below:

  1. I/p on this card supports upto 100VDC , my requirement for I/p is 45V-95V DC. So can i use it? what modification do i need to do for the same
  2. O/p on card is 12V upto 7A. but my requirement is o/p 12V 9A. So again can i use it? what modification do i need to do for the same?

 Thanks in Advance.

  Deeply awaiting your reply.