This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5026: Can't synchronize with external clock

Part Number: LM5026

The circuit is designed as the circuit in the datasheet.  The part of Q7 is SSM3K02T from Toshiba,C32 is 33pF,R35 is 10k. 

The pin 3  CS  of  LM5026 is connected to GND,  pin 13 COMP is floating .  As a result, the duty cycle of pin 8 outputA is maximum. Without the external clock, the frequency is about 350kHz. 

 When apply a signal to the Gate of Q7, the frequency of is not changed. The signal is 5V, 443kHz and  provided by a signal source. The waveform is below

CH1  is the external clock,  CH2 is the pin 8 OUTA of LM5026,  CH3 is the pin 15 SYNC of LM5026.  The input external clock is 443kHz,  however the ouput frequency is not changed, remaining about 350kHz. It seems the LM5026 is not  synchronized with the external clock.  From the CH3 waveform of Oscilloscope ,  the  voltage sometimes is below 0V which is confused.  

As the clk of LM5026 is unable to be seen, I have no idea about what is happened in the LM5026. Please help me with the problem ,thanks.