Hello,
I need to program the NVM to a different output then the defaults in the manufacturing stage using an external I2C programmer.
the power settings in all 3 of the part numbers listed in the datasheet will damage me design until I reprogram the NVM
1. How can I disable the device power outputs until I program the NVM to my power settings?
2. Is there a part number with only the I2C working - so I can program the NVM - but without any power outputs active?
Thanks