Part Number: UCC39002
Other Parts Discussed in Thread: UCC29002
Hi Team,
My customer is looking for load sharing solution for 54Vout server PSU, PSU's output power is ~kW level.
Do we have suitable solution?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Charles,
both UCC39002 and UCC29002 are suitable for this case. The only difference of UCC39002 and UCC29002 is the operation temperature range. And UCC29002 has wider operating temperature with -40~105degree.(UCC39002 with 0-70degree).
for 54V application, you can refer to UCC29002 datasheet Figure.5 High voltage application.
hope this helps you.