Hi,
I'm wanting to use tps54302 in some projects and would like some help to know if the schematic is correct
INPUT: 12VDC TO 24VDC
OUTPUT: 3V3 2.5A
EN does not connect to anything?
thank you so much!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm wanting to use tps54302 in some projects and would like some help to know if the schematic is correct
INPUT: 12VDC TO 24VDC
OUTPUT: 3V3 2.5A
EN does not connect to anything?
thank you so much!!
Hi ,
pls find my comments below.
1. Add one 0.1uF cap as close to VIN-GND.
2.You can float the EN pin , devices would enable as there is internal resource to pull up this en pin voltage.
3.Not sure the 3A inductor details , normally we would recommend to select a inductor with Isat >= OC value , Itemp >= 3A for tps54302.
BRs,
Young