This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Battery Charger IC Recommendations

Other Parts Discussed in Thread: BQ24133

Hello,

I'm currently in the concept phase of a project and thought it useful to reach out and invite your recommendations (in addition to my ongoing research).

My design will feature a 5V DC barrel jack input (via external desktop PSU) with battery backup power, most likely to be a standard 3.7V Lithium Polymer cell, with the potential for x2 instances of this cell.

The primary supply will be the external desktop PSU, but upon disconnection, the battery will need to seamlessly keep the device powered, UPS-style as it were.  The device typical operational current is expected to be ~3A.

The battery will need to be charged to capacity whenever the primary external PSU is connected, which is the principle mode of operation.  It is not expected a high charge rate will be required for the battery.

Ideally, I'd like the control interface to be I2C, though I'm happy to consider Standalone also.

The only other consideration, this is likely to be a reasonably dense design, so a single chip solution would be great.  I'm happy to consider two-chip solutions also though.  Any recommended parts will need to have current availability from TI or other vendors as I'll be looking to put this design out for Manufacture within 4 or 5 weeks.

Many thanks in advance! 

  • Peter,

    It appears that you need a charger with traditional power path that provides the input 5V to the system and then reverts to 1S battery when 5V is removed.  If your system can run on battery (i.e. doesn't need the battery voltage boosted to 5V), the standalone BQ24133 should work and there is some inventory with more expected first week of May.  

    Regards,

    Jeff

  • Hi Jeff, thank you kindly for your reply. Fantastic, thank you for providing this recommendation. I am using a Lithium-Ion battery that will provide 3.7V output voltage, so will require boost to 5V. Do you have any recommendations with this in mind?

    Many thanks.

  • Hi Peter,

    Unfortunately, I no longer support TIs boost converters.  I recommend creating a new post with the boost converter input voltage range, desired output current and voltage.  When placing it after the charger, the boost converter needs 100% duty or pass through mode so that it passes the 5V input when applied.  It also needs to have very fast startup.  You could also place it in series with the charger external BATFET.   The converter also needs to be able to startup with a pre-biased output.   

    Regards,

    Jeff

  • Hi Jeff,

    Thank you kindly for your response there.  Could I confirm also, are there no single-chip TI battery charger solutions also able to boost battery voltage, or is the currently no availability of any relevant chips?

    I am happy to use a two-chip solution, so I will also create a new post as per your recommendation there, Jeff.

    Many thanks.

  • Hi Peter,

    Our chargers do not integrate the boost function.  

    Regards,

    Jeff