AC to AC converter with below specs-
Input: 100V to 250V AC, 50/60HZ
OUTPUT: 50V TO 110V AC, 300VA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
AC to AC converter with below specs-
Input: 100V to 250V AC, 50/60HZ
OUTPUT: 50V TO 110V AC, 300VA
Hi Sagar,
Not sure what you are trying to do here. We do have PMP9640 which can take the AC input down to a DC bus, then if you follow that with PMP9461, this might be what you are looking for.
If you don't require precision regulation a simple 2:1 transformer might be what you need.
I hope this gives you some ideas.