hello there,
i have here a custom board with a BQ25895. on the pin ILIM there is a resistor with 180 ohm to ground.
according to the datasheet (section 8.2.12) i can monitor the input current (the current in VBUS) by measuring VILIM (what i do with an ADC on ILIM pin). according to formula 4 i shold be able to calculate the input current.
but i don't understand what KILIM is.
the electrical characteristics notes that it is a value between 320 and 390. which leads to a quite big difference in the calclated input current.
i measured the input current on VBUS (360mA) and the voltage on ILIM when charging is enabled (178mV). then i calculated back the KILIM with the above formula. but i get a KILIM of approx. 290.
can someone pleas help me with my understanding of KILIM.?
Is this a constant? how can i determine the value to calculate my input current? shall i take min, max or typical value of KILIM to calculate the current?
Did I understand it correctly that VILIM has a maximum voltage of 0.8V?
thank you very much for your help!
best regards peter