Other Parts Discussed in Thread: TPS629206, TPS629210, TPS629203
hi team,
I´m currently helping customer selecting some components and would appreciate some inputs on below requirements:
|
Parametreler |
-5V ic |
|
Part |
Active, suitable for new designs |
|
Stock |
Available |
|
Function |
Step-Down |
|
Minimum Input Voltage (V) |
3 |
|
Maximum Input Voltage (V) |
12 |
|
Minimum Output Voltage (V) |
Fixed -5V |
|
Maximum Output Voltage (V) |
- |
|
Current (A) |
0,05 |
|
Output Type |
Fixed |
|
Output Number |
1 |
|
Enable/ Disable Function |
Available |
|
Temperature °C |
At least the following range should be ok. |
|
Target ripple mV |
<1mV |
|
EMC emission |
Complies, |
|
EMC immunity |
Complies, |
It is used for the Opamp Supply, maybe you can consider this condition. (0<Iout<10mA)
Ive promoted TPS63710 but in this current out regime, TPS63710 efficiency is almost zero.
please let me know what could be recommended here.
Thanks!
Regards,
Brian