Other Parts Discussed in Thread: TPS543C20
Hi Team,
I have two questions while running TPS543C20A Webench simulation. Basic operating condition is as below and I also attach the Webench reports.
VinMin = 10.8V
VinMax = 13.2V
Vout = 0.85V
Vout Sch = 0.85V
Iout = 40.0A
Fsw = 500kHz
1. How is the duty cycle determined in the report? I run it with Ta = 25 degC and with Ta = 55 degC. And duty is 7.182% and 7.301% each. I expected the duty would be 6.44~7.87% (0.85V/13.2V~0.85V/10.8V).
2. Why the duty is different in the two reports - only difference in setup is Ta 25 degC vs 55 degC.
3. I basically want to see the TPS543C20's Tj performance along with Vout and Iout change (non-A version). Do you expect the Tj would be same or similar to TPS543C20A simulation result?
WBDesign58_1.pdfWBDesign58_2.pdf
Thank you!