This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25798BKUPEVM: charge 4s LiFePO4

Part Number: BQ25798BKUPEVM

Hi,

I need support to understand the correct config to be able to charge 4s LiFePO4 cells.

I'm able to charge 1 and 2 cells. No luck with 3s and 4s (both 750kHz and 1.5MHz config).

ILIM_HIZ is set to 500mA.

I've checked that 4s 1.5MHz PROG = 17.4k 

I'm using VAC1 input from 5V to 20V.

I tried also to bypass VAC to VBUS.

What I always get is STAT pin in fault condition (1Hz toggling).

The BQ on the evaluation board is marked as PX2579X.