Hello, I am using the TPS61023 boost IC for my design. In the boost circuit, the inductor is used between the input and SW pin of IC, if I am short this inductor then it damaged the IC. Please provide the solution so that I can protect my IC from damage. The input of the Boost IC is 3.3V-4.2V and the output is 4.2V.