This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5146: Suggestion on Capacitor/Inductor/Resistor for COMP

Part Number: LM5146
Other Parts Discussed in Thread: LM5145

Dear, 

We are using LM5146 with the PD controller. The output voltage will be different depending on the configure. 

Here is the list of different output voltage

OUTPUT

5V

3A

9V

3A

15V

3A

20V

2.25A

  • The frequency is set to 400khz
  • The input voltage is 37V ~ 54V. 
  • FB pin is using 200k and 38.3K resistors. 

 Since in this application, the output voltage will be different, may I have your suggestion on the values of the capacitor/Inductor/Resistor for COMP pin? 

Thank you.