This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53659: Power Sequencing

Part Number: TPS53659
Other Parts Discussed in Thread: TPS53679, , TPS536C7

Hi Team, 

I had a quick question on the TPS53659, TPS53679, and TPS536C7 Power Sequencing.

Can you confirm that it is okay for 3.3V for these controllers to come up before the 5V for the power stages? It’s my understanding that this is okay as long as the enable of controller is the last one being powered, is that right?


The customer mentioned some feedback that "- If the +3V3_VRD come up first before +5V_VRD, the controller shuts down the PWM pin due to it does NOT detect the power stage presented." So wanted to clear up any confusion.

Thank you, 
Delaney