Other Parts Discussed in Thread: UCC256402, UCC28740, UCC25600, UCC28782, UCC28780
Hello:
While looking into the eval kit of UCC256404 LLC controller, is there a possibility of starting it up from the input power line itself as it is done in almost all controllers.
In the Web BAsed design, there is "battery" like symbol. Of it is not practical to do so is any commercial product.
Also, some applications show an elaborate "small" converter to get 12v from AC. As in the Eval kit.
The paradox is that the present design using UCC256404 will be itself a " small" converter of 30W, cost-competitive. Furthermore, the dc power input is 600V. The paradox becomes acute since small biasing converters are flyback...which can start by trickle current from the input line...but 600V input DC is problematic in flyback mode even if we can use 1200V device.
It is not an option here.
What approaches have you tried and is there an App Note on the startup for UCC256404?
Any help in the matter will be appreciated.
r