This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3824: The same function recommand with MAX6318LHUK26DX-T

Part Number: TPS3824


Hi experts,

Do we have the suitable socket to the MAX6318LHUK26DX-T? I find TPS3824 has same function, same pinout, but only 200ms delay time. My customer selected the MAX6318LHUK26DX-T becasue of 1.6s delay time.

Customer need to keep RESET high level grearter than 500ms for ensuring power start-up time.

BR,

Gordon