Other Parts Discussed in Thread: UCC25640EVM-020, UCC28064EVM-004, , UCC256404
Hi Tech Support,
Designing power supply for Avionics application with 400Hz line frequency. Using PMP30763 as a design guide.
Also working with UCC25640EVM-020 and UCC28064EVM-004 evaluation boards. At this time running tests at about 60W load and 115VAC input.
I would like help with is the following. When running the PFC evaluation board (UCC28064EVM-004) with a resistive load, Power Factor remains high (above 90%) with a 400Hz line frequency.
Even at 800Hhz, power factor remains high.
Next step, I connect the PFC evaluation board to the LLC evaluation board (UCC25640EVM-020). Resistive load is connected to the LLC board and adjusted for the same power as before.
Running at 60Hz Power Factor is high (0.942). But as line frequency is increased the power factor drops. At 400Hz power factor is very low at 0.49.
What might be happing here causing low power factor when the LLC power supply is used? Again when running at 60Hz with the LLC board, PFC power factor is high. Also with just the PFC board, Power Factor remains high at 400Hz.
Regards,
Stuart