This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
We're considering using the TPS7A7200QRGWREP in place of the TPS7A7200RGWT due to supply constraints. Whilst the two part are identical in almost all facets the only significant difference I see is the Minimum Junction and storage temperature. TPS7A7200QRGWREP has a Junction temperature range of -40°C toe 150°C compared to the TPS7A7200RGWT, which has a junction temperature range of -55°C to 160°C.
Thank you.
Hello,
For this device, operating temperature and the Operating junction temperature (TJ) are used synonymously and to refer to the same thing. Since the abs max TJ ratings for the two devices are different, please ensure that the application does not violate these ratings. The EP and Non- EP versions typically are built of different materials and/or tested differently and therefore could have different ratings. Thanks!
Regards,
Srikanth